S32K344 eMios Signal Measurement Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 eMios Signal Measurement Problem

Jump to solution
5,916 Views
tsirkunenkoa
Contributor II

Hi,

we need to use the Period and Duty Cycle measurement functionality of the eMios module. However, when trying to apply PWM to the corresponding port - the results of corresponding measurement functions are zeros. Is it possible to verify if the eMios ICU works in this mode?

Setup:
S32K3X4EVB-Q172 board. The eMios PWM example was taken as a base one, ICU module was added on top with corresponding functions:

tsirkunenkoa_0-1652438746317.png


The corresponding additional pin for measurement was setup:

tsirkunenkoa_1-1652438825635.png

A jumper wire with no resistance was connected between the pins in the following way (shown with red line):

tsirkunenkoa_2-1652438989993.png

ICU module configuration:

tsirkunenkoa_3-1652439088302.png

 

tsirkunenkoa_4-1652439103038.png

RTD version:

tsirkunenkoa_5-1652439236354.png


I can attach the project archive upon request.

Thank you in advance!

0 Kudos
Reply
1 Solution
5,910 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @tsirkunenkoa,

You can refer to this example:

https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-Example-Emios-Icu-IPWM-measurement-DS34-RTD...

It uses customized ISR, but the configuration of the drivers should be very similar to your usecase.

 

Regards,

Daniel

 

View solution in original post

0 Kudos
Reply
6 Replies
5,911 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @tsirkunenkoa,

You can refer to this example:

https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-Example-Emios-Icu-IPWM-measurement-DS34-RTD...

It uses customized ISR, but the configuration of the drivers should be very similar to your usecase.

 

Regards,

Daniel

 

0 Kudos
Reply
5,902 Views
tsirkunenkoa
Contributor II

Hello @danielmartynek,

Thank you for your quick reply!

I have tried your example and everything is working! I suppose that these measurement functions should only be called from the interrupt then, right? If so, it would be nice if this was mentioned in the function comments.

Also, I would normally just give the "Interrupt Control" driver the corresponding "EMIOS1_5_IRQ" function handler, however it seems like the only solution currently is to do it the way you said (by creating interrupt handler ourselves) since there is no callback function that can be setup for Singal Measurement mode.

Have a nice day!

0 Kudos
Reply
5,893 Views
danielmartynek
NXP TechSupport
NXP TechSupport

You can leave the ISR to the driver.

But as you said, there is no notification, and it would have to be polled.

 

BR, Daniel

 

0 Kudos
Reply
5,739 Views
ywjack
Contributor III

Hello NXP Technical Support: I want a DEMO about the EB MCAL configuration ICU module is configured to input capture PWM duty cycle, because I found that the ICU I configured cannot trigger interrupts, I am using a S32K146 microcontroller, EB tresos version is 27.1.0. So I want a demo to compare and see.

0 Kudos
Reply
5,890 Views
tsirkunenkoa
Contributor II

Ok, I see that it shouldn't be necessarily called from an interrupt, but can be checked in a for loop until the period is not zero.

Regarding the notification, it would be great if this functionality could be added. Otherwise, if the asynchornous measurement is required - the developers would need to write their custom ISR handler. The main problem here is that this ISR handler is used by other channels as well if they are configured (e.g. EMIOS1_5_IRQ will handle 0, 1, 2, 3 channels) and in this case we would need to differentiate from which channel the interrupt came from and act accrodingly, e.g. the following way:

if ( 0U != ((Emios_Ip_paxBase[1]->CH.UC[0].S) & (uint32)eMIOS_S_FLAG_MASK)

 But anyway, I hope the notifications for measurements or channels will be added soon.

Thanks again and I will continue as is.

0 Kudos
Reply
5,880 Views
danielmartynek
NXP TechSupport
NXP TechSupport

You are right.

Let me create a ticket to the RTD team.

 

Regards,

Daniel