S32K344: eMIOS triggering the BCTU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344: eMIOS triggering the BCTU

1,198件の閲覧回数
Samuel_DCosta
Contributor III

Hi,

I need the eMIOS to trigger the BCTU without interrupting the CPU. Currently, I am using the eMIOS GPT driver but I realized that if I remove the interrupt of eMIOS then triggering the BCTU stops. 

Is it possible to trigger the BCTU via the eMIOS without CPU intervention? 

0 件の賞賛
返信
1 返信

1,167件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Yes! It is possible to trigger the BCTU via the eMIOS without CPU intervention, you can refer to the 4.2.4. Analogue data capturing from app note AN13767. Also you can check the config in its respective software in MCSPTE1AK344 page.

Hope it helps you.

Have a nice day!

0 件の賞賛
返信