S32K344 cannot download programs to flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 cannot download programs to flash

1,492件の閲覧回数
xuan
Contributor I

HI,

What causes this? The chip is locked?

PEmicro Interface detected - Flash Version 11.37

CMD>RE

Initializing.
Target has been RESET and is active.
CMD>CM D:\anzhuang\S32DS35\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_5.7.8.202404031741\supportFiles_ARM\NXP\S32K3xx\nxp_s32k344_1x32x1012k_hse_disabled.arp

Initializing.
Initialized.

;version 1.02, 01/18/2024, Copyright 2024 P&E Microcomputer Systems, www.pemicro.com [S32K3x4_hse_disabled]

;device nxp, s32k344, 1x32x1012k,desc=hse_disabled

;begin_cs device=$00400000, length=$003F4000, ram=$20400000

Loading programming algorithm ...
Done.
Programming sequency is : erase, blank check, program, and verify {default}
CMD>VC
Verifying object file CRC-16 to device ranges ...
block 00400000-0040A86B ...
Calculated CRC-16 does not match block. (File = $3018, Device = $8583)
Current content of flash does not match application to be programmed

CMD>EM

Erasing.

Module could not be erased.
Error Erasing flash of device
Error occured during Flash programming.

0 件の賞賛
返信
2 返答(返信)

1,451件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @xuan,

Were you able to use the .elf file with board before? Does this happen with an example project? You can also try the emergency full chip erase:

Julin_AragnM_0-1719938807313.png

Best regards,
Julián

0 件の賞賛
返信

1,463件の閲覧回数
Djuric
Contributor III

Did you manage to solve the problem?

0 件の賞賛
返信