Recovering from Secure Boot on S32K3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recovering from Secure Boot on S32K3

1,266 Views
end48
Contributor I

Hello,

I'm currently implementing secure boot on a S32K310. I've got two questions:

  1. In case I configure secure boot on an SMR, how can I recover if the code in this SMR becomes corrupted? Do I need to flash with a debug probe the non corrupted firmware again? Is there another way?
  2. In case I need to modify the code in the SMR after activating the secure boot (during development typically), can I disable secure boot before updating the code and reconfigure secure boot on the new code?

Thanks,

Benoit

0 Kudos
Reply
1 Reply

1,205 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) You will have to update SMR if possible.

2) Once the secure boot is enabled, it can't be disabled.

0 Kudos
Reply