S32K344 can connect Jlink but not debug with Jlink or PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 can connect Jlink but not debug with Jlink or PE

143件の閲覧回数
MountQomolangmaclimber
Contributor I

Hi everyone,

I met a problem with my S32K344. It can connect JLINK and can be erased via JLINK. But it cannot  neither debug with JLINK or PE, nor run programme normally. For example, there is a programme about LED twinkling, I download it in S32K344 via JLINK, but the led does not work.

The cause may be follow:

In a project of S32K358, I used PE for debugging and forcibly changed the configuration of PE from S32K358 to S32K344. Then I clicked Dubug, which caused the chip to be unable to continue to be used normally.

The above is entirely due to personal negligence. I hope my S32K344 return to normal, but I have no choice.

So I ask everyone for help. Thank you!

Here are some pictures about debugging:

MountQomolangmaclimber_0-1758942999453.png

 

MountQomolangmaclimber_1-1758943322734.png

Then I connect it with Jlink:

MountQomolangmaclimber_2-1758946503803.png

MountQomolangmaclimber_3-1758946596649.pngMountQomolangmaclimber_4-1758946638006.png

 

Then I debug with PE, there are some pictures:

MountQomolangmaclimber_5-1758946796345.pngMountQomolangmaclimber_6-1758946854528.png

MountQomolangmaclimber_7-1758946913043.png

As you can see, I cannot debug with PE or Jlink. So confused.

If you have any solution or advice, please reply soon. Thank you!

 

0 件の賞賛
返信
2 返答(返信)

115件の閲覧回数
MountQomolangmaclimber
Contributor I

Oh, although it can be debugged in IAR, but when I turn off the power, and turn on the power, it does not work normally. I doubt that IAR debugs my S32K344 in RAM not flash.

0 件の賞賛
返信

136件の閲覧回数
MountQomolangmaclimber
Contributor I

Amazing!

It can be debugged in IAR!

MountQomolangmaclimber_0-1758948307092.png

 

0 件の賞賛
返信