S32K344-WB (WhiteBoard) EVB source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344-WB (WhiteBoard) EVB source code

ソリューションへジャンプ
2,905件の閲覧回数
jwkang
Contributor III

I purchased S32K344-WB EVB.
I operated EVB by referring to the example in another link on the site.
( https://community.nxp.com/t5/S32K/S32K344-Whiteboard-Example-Project/m-p/1500850 )

After running Debug using Example, the EVB operation that was originally built in when purchased disappeared.

I want to return EVB to its initial state.
Please share the source code or binary file included.

0 件の賞賛
返信
1 解決策
2,881件の閲覧回数
StephenDu
NXP Employee
NXP Employee

hi, jwkang

I think this is what you want, please download and install it.

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,853件の閲覧回数
jwkang
Contributor III

Thank you for your support.

0 件の賞賛
返信
2,882件の閲覧回数
StephenDu
NXP Employee
NXP Employee

hi, jwkang

I think this is what you want, please download and install it.

 

 

0 件の賞賛
返信