S32K344 SPI with External Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 SPI with External Flash

Jump to solution
2,566 Views
S3RD4R
Contributor I

Hello all,

I am just a beginner for S32K344 and trying to communicate with external flash. I control NSS with GPIO myself. I try to read device's ID which consists of 2 step:

1 - Send ID read command  to the external flash

2 - Read 3 bytes back from the external flash

 

I send the following commands;

FLASH_NSS_LOW();

Spi_SetupEB(0u, CommandArray, NULL, 1u);
Spi_SyncTransmit(SpiConf_SpiSequence_FlashSpiSequence);

Spi_SetupEB(0u, NULL, ReadArray, 3u);
Spi_SyncTransmit(SpiConf_SpiSequence_FlashSpiSequence);

FLASH_NSS_HIGH();

Is this sequence correct? Because whenever i send Spi_SyncTransmit command, i receive an abnormal pulse. I checked the forums i came to this topic;

https://community.nxp.com/t5/S32K/S32K3-SPI-CS-problem-when-using-GPIO-to-simulate-CS/td-p/1564367

Therefore, i removed FLASH_NSS_LOW to Lpspi_TransmitTxInit after State->TxIndex = 0u;

 

So, when i send the first command the pulse is ignored, however when i send the second Spi_SyncTransmit another pulse just messes up my command. 

 

I would appreciate any help at this stage.

Thank you,

 

 

 

 

 

0 Kudos
Reply
1 Solution
2,467 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi @S3RD4R ,
Sorry for the late response, this topic was missed in my support list,
Your sequence seems correct if you use external buffer, despite that I'm not sure what is FLASH_NSS_LOW and FLASH_NSS_HIGH in your source code.
If the issue you faced is the same with https://community.nxp.com/t5/S32K/S32K3-SPI-CS-problem-when-using-GPIO-to-simulate-CS/td-p/1564367, the simple workaround is remove macro ERR_IPV_LPSPIV2_0001 from the compiling process. 

View solution in original post

0 Kudos
Reply
1 Reply
2,468 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi @S3RD4R ,
Sorry for the late response, this topic was missed in my support list,
Your sequence seems correct if you use external buffer, despite that I'm not sure what is FLASH_NSS_LOW and FLASH_NSS_HIGH in your source code.
If the issue you faced is the same with https://community.nxp.com/t5/S32K/S32K3-SPI-CS-problem-when-using-GPIO-to-simulate-CS/td-p/1564367, the simple workaround is remove macro ERR_IPV_LPSPIV2_0001 from the compiling process. 

0 Kudos
Reply