S32K344 SAF FCCU Fault Injection never returns

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 SAF FCCU Fault Injection never returns

ソリューションへジャンプ
1,821件の閲覧回数
lluo
Contributor IV

Hi,

I am currently working with s32 saf demo. I got the demo after installing the S32 SAF framework version S32K3_SAF_1.0.4_EVAL_D2312. 

lluo_1-1709890721934.pnglluo_1-1709890721934.png

During running the demo, I found out when I tried to inject the following fault:

eMcem_InjectFault( EMCEM_DCM_NCF_1_AD_EDC_ERR_OUT )

the function never returned. After a detailed look,I found out that the program got stuck in the following place:

lluo_2-1709890862102.pnglluo_2-1709890862102.png

It failed writing to the register.

Do you probably have any idea about why this happened? Thank you in advance. 

 

 

 

0 件の賞賛
返信
1 解決策
1,790件の閲覧回数
lluo
Contributor IV

The issue is solved by the following configuration:

lluo_0-1710210406292.pnglluo_0-1710210406292.png

In the Reaction Type section, select "No reset reaction" instead of "Short reset reaction".

The issue can be closed.

 

元の投稿で解決策を見る

タグ(1)
0 件の賞賛
返信
1 返信
1,791件の閲覧回数
lluo
Contributor IV

The issue is solved by the following configuration:

lluo_0-1710210406292.pnglluo_0-1710210406292.png

In the Reaction Type section, select "No reset reaction" instead of "Short reset reaction".

The issue can be closed.

 

タグ(1)
0 件の賞賛
返信