S32K344 Qspi_Ip_Example Qspi_Ip_Init timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 Qspi_Ip_Example Qspi_Ip_Init timeout

5,145件の閲覧回数
Li_Chen
Contributor III

I'm working on the S32K344 Qspi_Ip_Example for S32K3XXEVB-Q172 51972 PCB RevA SCH RevA board. Qspi_Ip_Example_S32K344_Debug_FLASH_PNE is used as debug configuration. After running,

Qspi_Ip_Init(instance, &QspiConfigSet_VS_0_paFlashCfg[0], &QspiConfigSet_VS_0_paFlashConnectionCfg[0]); in the main file gets timeout.

I'm using S32 DS 3.4 and RTD SW version 2.0.0, build vresion S32K3_RTD_2_0_0_D2203_ASR_REL_4_4_REV_0000_20220331

0 件の賞賛
返信
6 返答(返信)

5,129件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you provide example code showing the issue, letting us to the debug it? Thanks

0 件の賞賛
返信

5,115件の閲覧回数
Li_Chen
Contributor III

It's generated by IDE. I attached the main file here. Here are my further progress, I tested three S32K3x4EVB-Q172 boards, only one could pass the test. The others are stuck in the  Qspi_Ip_Init function and eventually timeout

0 件の賞賛
返信

5,057件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Are all these used board of same revision?

0 件の賞賛
返信

5,051件の閲覧回数
Li_Chen
Contributor III

They are the same revision: 700-51972 REV A.

0 件の賞賛
返信

4,968件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

On my side it runs normally. I will try to ask whether they are known issues with this board or this SW example configuration.

0 件の賞賛
返信

4,973件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I will try to test it on my side. In the meanwhile I would like to ask whether you have tried newer version of S32DS or RTD?

Described behavior is interesting, I am not sure if consider it rather as HW or SW issue.

0 件の賞賛
返信