Hi, I'm having some problems
(RTD Version: SW32K3_S32M27x_RTD_R21-11_4.0.0)
1. Intergrate MCAL Gpt Example to S32DS, and make sure no errors within Build process
2. In function Power_Ip_PMC_PowerInit(), after running line 316, the debug process invoke error, during this IP_PMC->CONFIG'value from 0 to 1
3. Detailed error and EB config
How can I fix it?
Hi @Yown,
How do you power the V15 domain of the MCU?
It can be powered directly from an SBC/PMIC or generated by the external ballast VC_BJT.
You need to configure the driver accordingly.
Regards,
Daniel