S32K344 MCU LPUART configuration issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 MCU LPUART configuration issue

2,288件の閲覧回数
nitish2
Contributor I

Hi Team

I am working on one of the projects that usea S32K344 MCU. In that i am facing UART working problem in which i am not able to communicate via UART. Can you please provide solution for this or uart example code ?

Platform i am using is S32 Design Studio v3.5(Ubuntu 20.04 LTS).

Project : RTD AUTOSAR 4.4
* Platform : CORTEXM
* Autosar Version : 4.4.0
* Autosar Revision : ASR_REL_4_4_REV_0000
* SW Version : 1.0.0
* Build Version : S32K3_RTD_1_0_0_D2110_ASR_REL_4_4_REV_0000_20211007

************************************************************************************************************

0 件の賞賛
返信
3 返答(返信)

2,213件の閲覧回数
nitish2
Contributor I

Hi
I tried over windows laptop for UART issue. In windows i could open and configure .mex file for UART. Don't know why in ubuntu laptop i could not do the same.

0 件の賞賛
返信

2,239件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I don't know the specific situation of S32DS v3.5 in Ubuntu, because I have only used Windows.
As far as I know, S32K3 RTD 1.0.0 was released 3 years ago. Logically speaking, and the current S32DS v3.5 should be S32K3 RTD 4.0.x.
Will you see examples of S32K3 RTD after Online Package Installation it on your S32DS v3.5?
File -> New -> S32DS Project from Example
LpuartFlexio_Uart_Ip_Example and Uart_Example.


Best Regards,
Robin

0 件の賞賛
返信

2,286件の閲覧回数
nitish2
Contributor I

hi team
I am attaching the S32K344.mex file for the reference in which LPUART configs. can be found.

0 件の賞賛
返信