S32K344 MCU LPUART configuration issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 MCU LPUART configuration issue

2,312 Views
nitish2
Contributor I

Hi Team

I am working on one of the projects that usea S32K344 MCU. In that i am facing UART working problem in which i am not able to communicate via UART. Can you please provide solution for this or uart example code ?

Platform i am using is S32 Design Studio v3.5(Ubuntu 20.04 LTS).

Project : RTD AUTOSAR 4.4
* Platform : CORTEXM
* Autosar Version : 4.4.0
* Autosar Revision : ASR_REL_4_4_REV_0000
* SW Version : 1.0.0
* Build Version : S32K3_RTD_1_0_0_D2110_ASR_REL_4_4_REV_0000_20211007

************************************************************************************************************

0 Kudos
Reply
3 Replies

2,237 Views
nitish2
Contributor I

Hi
I tried over windows laptop for UART issue. In windows i could open and configure .mex file for UART. Don't know why in ubuntu laptop i could not do the same.

0 Kudos
Reply

2,263 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I don't know the specific situation of S32DS v3.5 in Ubuntu, because I have only used Windows.
As far as I know, S32K3 RTD 1.0.0 was released 3 years ago. Logically speaking, and the current S32DS v3.5 should be S32K3 RTD 4.0.x.
Will you see examples of S32K3 RTD after Online Package Installation it on your S32DS v3.5?
File -> New -> S32DS Project from Example
LpuartFlexio_Uart_Ip_Example and Uart_Example.


Best Regards,
Robin

0 Kudos
Reply

2,310 Views
nitish2
Contributor I

hi team
I am attaching the S32K344.mex file for the reference in which LPUART configs. can be found.

0 Kudos
Reply