S32K344 HSE Demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,877件の閲覧回数
ValTek
Contributor III

Hi,

I downloaded the:

HSE_FW_S32K3XX_0_0_14_0

HSE_DEMOAPP_S32K3XX_0_0_14_0

I'm trying to test HSE. Following the guide, I tried to download the demo app (step 1):

VinsBos_0-1655976589850.png

Unfortunately I found this in trace32:

Select SOC TAP
IDCODE: 0x0996001D
INFO: SW-DP DPv2 enabled; SwitchToSwd=TryAll->JtagToSwd; TARGETSEL=0xffffffff; DPIDR=0x6ba02477
file 'C:\T32\demo\arm\flash\long\s32k3x4.bin' (Binary) loaded.
FLASH algorithm did not execute completely

The script ends with the correct popup but clearly the operation is not ok. I check the memory and nothing happened.

I use the demo board Q172 (using JTAG port).

I check the bins in my T32 Long folder:

VinsBos_1-1655976892685.png

My T32 version: 

VinsBos_2-1655976965370.png

 

Maybe it could be helpfull information...

 

0 件の賞賛
返信
1 解決策
4,842件の閲覧回数
ValTek
Contributor III

Nevermind: I resolved it using a different script from another project. Probably it was something from the debugger.

Unfortunately I encounter another problem (I'll open a new thread).

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,843件の閲覧回数
ValTek
Contributor III

Nevermind: I resolved it using a different script from another project. Probably it was something from the debugger.

Unfortunately I encounter another problem (I'll open a new thread).

0 件の賞賛
返信