S32K344 - DIO Configuration support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K344 - DIO Configuration support

1,438件の閲覧回数
Er_AK
Contributor I

MBDT DIO example used and working fine. When used to generate other pin, made the same settings as per the example except port and channel ID. It not generating ant error, but it is not generating output. Is there any document which help to use DIO?

0 件の賞賛
返信
1 返信

1,430件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hmm, the usage is quite simple here. Are you sure you have device package which supports the pin you would like to configure?

DIO documents are inside the driver package in folder doc.

petervlna_0-1719300961481.pngpetervlna_0-1719300961481.png

If you share more details I can try to generate the code for the requested pin.

Best regards,

Peter

 

0 件の賞賛
返信