S32K342 LPSPI Async Transmit for 64 Byte frames having issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K342 LPSPI Async Transmit for 64 Byte frames having issues

2,313 Views
bbaskii
Contributor II

Hi NXP Team,

I am using LPSPI3 in S32K342 and my requirement is sending 64 byte frame at once using AsyncTransmit and interrupt enabled. I am facing issue with loss of data exactly at 12th frame which contains CRC information in the frame sequence. Because of that the slave is not processing the frame and getting error. Kindly help me to fix the issue.

Thanks In advance,

bbaskii

Tags (1)
0 Kudos
Reply
3 Replies

2,280 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @bbaskii,

Can you share the project.

If you don't want to post it here, you can create a ticket.

Do you monitor the bus with an oscilloscope?

How is the frame corrected on the bus?

 

Thank you,

BR, Daniel

0 Kudos
Reply

2,249 Views
bbaskii
Contributor II
Hi Daniel,

I have created a ticket and uploaded the project which i am using it for testing. Please help me to fix the problem. Thanks, bbaskii
0 Kudos
Reply

2,239 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @bbaskii, I see, thank you

 

0 Kudos
Reply