S32K328NHT1MJBSR MAPBGA289 Programming problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K328NHT1MJBSR MAPBGA289 Programming problems

1,420 Views
gary_yang
Contributor II

Dear sir:

We are a third-party programmer manufacturer.

Currently testing programming the S32K328NHT1MJBSR.

After successfully programming the customer's file, the J-Link connects successfully,

001.JPG

 

but Erase fails.

002.JPG

 

If programming random code, erasing and programming can be repeated.

This is our programming circuit.

003.JPG

 

 

Do you have any suggestions?

 

Thanks

Tags (1)
0 Kudos
Reply
3 Replies

1,349 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@gary_yang

Based on the error message, you are attempting to erase the HSE area, which is likely the cause of the erase/write failure.

0 Kudos
Reply

1,308 Views
gary_yang
Contributor II

Dear Sir:

After programming a specific file, it cannot be repeatedly erased and programmed.

The entire IC cannot be eraseed.

If it's a programming random code, it can be repeatedly erased and programmed.

What is the address of the HSE area?

 

Thanks

0 Kudos
Reply

1,296 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@gary_yang

I'm not sure if this is the cause; this is just my guess. It's also possible that the current sector is locked in your code.

However, regarding the HSE memory address:

int_pflash : ORIGIN = 0x00400000, LENGTH = 0x007D4000 /* 8191KB - 176KB (sBAF + HSE)*/

Last 176KB reserved for HSE, that is: 0x00BD4000~0x00BFFFFF。

 

I suggest you contact SEGGER's technical support.

https://www.segger.com/support/technical-support/

 

 

0 Kudos
Reply