S32K324 inter core communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K324 inter core communication

1,348件の閲覧回数
chuanlin
Contributor III

chuanlin_0-1684130212665.pngchuanlin_0-1684130212665.png

Hi,It is seen in the document that core0 can trigger the interrupt of core1. Is there a demo for using this method?

 

0 件の賞賛
返信
1 返信

1,336件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi chuanlin,

The name of this document is S32K324_Dual_Core_Basics_v1.2? This document does not seem to be open to the public, where did you get it from? The training should have a demo called s32k324_dualcore_demo_20220524.zip that contains what you need. 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信