S32K324 -gptp stack version 0.9.0 AS master sometimes send PeerDelayRq package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K324 -gptp stack version 0.9.0 AS master sometimes send PeerDelayRq package

ソリューションへジャンプ
1,506件の閲覧回数
Nancy_LAN
Contributor II

dear support.

        the customer used the version of the gptp is 0.9.0,the S32K324 as master, sometimes S32K324 sends PeerDelayRq package. but the PC (Slave) can't respond the PeerDelayRq package. why should master send PeerDelayRq package?

Nancy_LAN_0-1749018682405.png

 

 

       

タグ(1)
0 件の賞賛
返信
1 解決策
1,418件の閲覧回数
janglos
NXP Employee
NXP Employee

Hello @Nancy_LAN, 

do I understand correctly that the issue is already resolved? Please confirm. 

Please note that NXP gPTP stack (or other IEEE 802.1as implementation) must be operated and correctly configured on each switch in the network for proper functionality. 

In case you need any further support, please let us know. 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,419件の閲覧回数
janglos
NXP Employee
NXP Employee

Hello @Nancy_LAN, 

do I understand correctly that the issue is already resolved? Please confirm. 

Please note that NXP gPTP stack (or other IEEE 802.1as implementation) must be operated and correctly configured on each switch in the network for proper functionality. 

In case you need any further support, please let us know. 

0 件の賞賛
返信
1,457件の閲覧回数
janglos
NXP Employee
NXP Employee

Hello @Nancy_LAN, 

could you please share more info about the setup used? 

E.g., which EVB you're using, what is the counter-device (I guess Linux PC w/ ptp4l?), if there is any switch in between of EVB and PC, maybe a simple schematics of the setup incl. MAC addresses and gPTP roles configured.

Thanks!

0 件の賞賛
返信
1,434件の閲覧回数
Nancy_LAN
Contributor II
Hello janglos,
The hardware board is customers. there is a switch between PC and board.
The customer later reported that it was manually turned off the PeerDelayRq package.
thanks for your support.
0 件の賞賛
返信