S32K324 Ram allocation problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K324 Ram allocation problem

1,701件の閲覧回数
Jackson_Ping
Contributor II

Hi,all,

I am currently using the S32K324 chip,But I have some problems at the moment.

In the attachment of the S32K324 manual there is a file of memory allocation, where the size of SRAM0 and SRAM1 correspond to core 0 and core 1 respectively?Or does SRAM0 or SRAM1 of core 1 work?

My current situation is: the program is in core 0, and my SRAM 0 space is used up. Can I allocate more SRAM space by modifying the LD file? Take more SRAM1, for example.

0 件の賞賛
返信
2 返答(返信)

1,683件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

My current situation is: the program is in core 0, and my SRAM 0 space is used up. Can I allocate more SRAM space by modifying the LD file? Take more SRAM1, for example.

Yes, RAM is not linked to just one core. It sits on the bus common to both.

By modifying the linker you can allocate any RAM to core. Slaves on XBAR can be assigned to any master listed in reference manual.

petervlna_0-1706085511776.png

petervlna_1-1706085595962.png

 

 

Best regards,

Peter

0 件の賞賛
返信

1,681件の閲覧回数
Jackson_Ping
Contributor II

Hi,Peter,

 

Thank you for your answer.

 

Best Regards,

  Jackson

0 件の賞賛
返信