S32K322 RTC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K322 RTC

1,238 Views
Chinnan
Contributor II

Hi,

I'm Using the S32K322 100 Pin HDQFP microcontroller. In the reference manual pins 15 and 17 are mentioned external crystal. I plan to use an external 24MHz crystal in those pins for the fast clock. Could you please mention which pins are the external RTC crystal (32.768KHz) in the S32K322?   

@RTC 

0 Kudos
Reply
1 Reply

1,223 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Chinnan 

The SXOSC crystal pins (OSC32K_XTAL and OSC32K_EXTAL) for S32K322 100 Pin HDQFP are unavailable (refer to attached image). 

VaneB_0-1696275317365.pngVaneB_0-1696275317365.png

For more details on pin functionality, refer to S32K342_S32K341_S32K322_IOMUX.xlsx attached to the reference manual. 

 

B.R.

VaneB

 

0 Kudos
Reply