S32K322 Pin Mapping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K322 Pin Mapping

Jump to solution
2,058 Views
Nivya
Contributor I

Hi,

Can you provide me the output pin mapping of S32K322 [100-Pin].

How many pins can be used as PWM in the same?

Thank you

 

0 Kudos
Reply
1 Solution
2,026 Views
PavelL
NXP Employee
NXP Employee

Hi Nivya,

the pin mapping file S32K342_S32K341_S32K322_IOMUX.xlsx is stored as an attachment of S32K3xx MCU Family - Reference Manual  - Sign in is required. PWM count which can be used in the same time depends on pin usage of other peripherals and PWM configuration.

Best regards,

Pavel

View solution in original post

0 Kudos
Reply
1 Reply
2,027 Views
PavelL
NXP Employee
NXP Employee

Hi Nivya,

the pin mapping file S32K342_S32K341_S32K322_IOMUX.xlsx is stored as an attachment of S32K3xx MCU Family - Reference Manual  - Sign in is required. PWM count which can be used in the same time depends on pin usage of other peripherals and PWM configuration.

Best regards,

Pavel

0 Kudos
Reply