S32K314 ETHERNET application question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K314 ETHERNET application question

828 Views
Nuzz
Contributor I

about the S32K314 ETHERNET application question

1. The network module of the IC contains 1 Ethernet unit and 6 CAN channels. For the peripheral circuit design of this IC, is it necessary to use other independent transceiver IC to transmit the Tx and Rx signals of the S32K314 to the host computer?

 

 
 
 
 
 
0 Kudos
Reply
1 Reply

798 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Yes, for the S32K314 microcontroller, which includes 1 Ethernet unit and 6 CAN channels, you do need external transceiver ICs to interface with the physical layer of both Ethernet and CAN communication.

For CAN transceiver refer to https://www.nxp.com/products/interfaces/can-transceivers:MC_53485
For ethernet PHYs, NXP offers just Automotive PHYs (IEEE BASE-T1 compliant); https://www.nxp.com/products/interfaces/ethernet-/automotive-ethernet-phys:ETHERNET-TRANSCEIVERS

BR, Petr

0 Kudos
Reply