S32K312 linker_flash content confirmation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 linker_flash content confirmation

ソリューションへジャンプ
1,389件の閲覧回数
victory
Contributor V

Hi,NXP expert:

Please help confirm whether the content of linker_flash_s32k312.ld is feasible, and focus on confirming whether the contents of line 58 in Figure 1 and line 225 in Figure 2 are correct.

victory_0-1749622372881.png

                                          Figure 1

victory_1-1749622529556.png

                                            Figure 2

Thank you, please reply to the above!

 

0 件の賞賛
返信
1 解決策
1,360件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@victory

Yes, I don't see any problem with the two parts you mentioned.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,371件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@victory

There is a problem in the link file you provided.

The two segments have overlapping addresses.

Senlent_1-1749627757737.png

You can try to modify it like this

int_sram_shareable : ORIGIN = 0x20417C00, LENGTH = 0x00000400 - 0x10

 

0 件の賞賛
返信
1,367件の閲覧回数
victory
Contributor V

Hi,Senlent

Okay, there should be no other issues with the attachments linker_flash_s32k312.ld, right?

Thanks!

0 件の賞賛
返信
1,361件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@victory

Yes, I don't see any problem with the two parts you mentioned.

0 件の賞賛
返信