S32K312 Unified BootLoader Build Issue - RTD Version Query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 Unified BootLoader Build Issue - RTD Version Query

1,171 Views
DiaDev
Contributor III

Hello,

I am currently working with the following configuration:

  • S32DS for S32 Platform 3.5

  • S32K312 code, which I'm using for the S32K311

The following link is what I followed: S32K3-Unified-Bootloader-Build-Issue 

I am encountering issues related to building the S32K3 Unified Bootloader. Could you please let me know which RTD version is compatible with these configurations?

Any help would be greatly appreciated!

Thank you.

0 Kudos
Reply
1 Reply

1,142 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Those projects are develop based on S32K3 Real Time Drivers Version 2.0.0. Please follow the method mentioned in that link to install RTD 2.0.0 in S32DS v3.4. Do not install it in S32DS v3.5.

Best Regards,
Robin

0 Kudos
Reply