S32K312 Sample Project Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 Sample Project Error

Jump to solution
1,520 Views
JH_ZHANG
Contributor I

Dear NXP technical support team

I want to proceed with the project using S32K312. First time using S32K312.
So, I am studying using the example project.
I installed and compiled the S32K RTD AUTOSAR 4.4 Version 2.0.0 D2203 example project on the homepage.
However, compiling causes errors.
The contents are as shown in the picture below.

JH_ZHANG_0-1704675170439.png

 

Please let me know why this error occurs.
and How can I use the example project?
 
Do you have any reference notes on sequential methods of using examples?
 
thank you.

 

0 Kudos
Reply
1 Solution
1,503 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@JH_ZHANG

please click "Update Code" and then build it again,

Senlent_0-1704681536928.png

 

View solution in original post

0 Kudos
Reply
1 Reply
1,504 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@JH_ZHANG

please click "Update Code" and then build it again,

Senlent_0-1704681536928.png

 

0 Kudos
Reply