S32K312 SPI + DMA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 SPI + DMA

2,063件の閲覧回数
sergiverdaguerelausa
Contributor II

Hi everyone,

 

I amb working on SPI with DMA.

Without using DMA with “Lpspi_Ip_SyncTransmit” the transmission works properly but when I use “Lpspi_Ip_AsyncTransmit” only 6 bytes are sent and the transmission never ends.

I attach code:

uint8 u8_frame_reset [] = {102, 170, 170, 170, 170, 170, 166, 166, 255};

 

int main(void)

{

    /* Initalized clock */

    Clock_Ip_Init(&Clock_Ip_aClockConfig[0]);

    /* Initalized pin */

    Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);

    /* Initialize interrupt */

    IntCtrl_Ip_Init(&IntCtrlConfig_0);

    IntCtrl_Ip_ConfigIrqRouting(&intRouteConfig);

 

    /* Initialize DMA IP} Driver */

    (void)Dma_Ip_Init(&Dma_Ip_xDmaInitPB);

 

    /* Initalized spi using instance lpspi as a spi slave */

    Lpspi_Ip_Init(&Lpspi_Ip_PhyUnitConfig_SpiPhyUnit_0_Instance_0_BOARD_InitPeripherals);

   

    error = Lpspi_Ip_AsyncTransmit(&MASTER_EXTERNAL_DEVICE, u8_frame_reset, NULL, sizeof(u8_frame_reset), spi_callback);

 

    while(1){

 

    }

 

    return 0;

}

 

And configuration:

sergiverdaguerelausa_0-1690903222854.png

 

sergiverdaguerelausa_1-1690903222889.png

 

If I try to send 2 bytes, the bytes are sent but the transmision never ends.

No callbacks.

0 件の賞賛
返信
5 返答(返信)

2,003件の閲覧回数
sergiverdaguerelausa
Contributor II

Hi,

 

The issue is related to TX and RX of SPI.
Is allowed config TX with DMA and RX as interrupt?

 

Thank you,

 

Sergi

0 件の賞賛
返信

1,978件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

I'm sorry for the delay, I have been overloaded the last couple of days.

If you only need to send but not receive (you fill NULL for RxBuffer), then you can use half duplex transfers(refer to Lpspi_Ip_HalfDuplexTransfer_S32K312).

0 件の賞賛
返信

1,923件の閲覧回数
sergiverdaguerelausa
Contributor II

Hi Robin,

 

I think that isn't the same case. I will try to explain in more detail.
I want SPI x4 with DMA. But I have only 6 DMAs for SPI. Every SPI has Tx and Rx so I need 8DMAs.

I only need DMA for Tx channels so my idea is work with 4 SPIs Tx with DMA and Rx without DMA, by simple interrupt. But the S32Design Studio configurator doesn't allowed it.

 

Are there any possible solution without change microcontroller to get this?

- SPI Tx with DMA x4

- SPI Rx x4 (DMA not needed)

 

Regards,

 

Sergi.

0 件の賞賛
返信

1,883件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

But the S32CT will report Issue: The SpiPhyUnitAsyncUseDma is checked, it implies that the DMA channels are activated and selected. Please enable SpiPhyTxDmaChannel, SpiPhyRxDmaChannel.

Please enable SpiPhyTxDmaChannel, SpiPhyRxDmaChannel.png

0 件の賞賛
返信

2,023件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

See the discussion in LPSPI Chip Select always is LOW (active state), where the project Lpspi_Flexio_Ip_Transfer_S32K344_Update.7z may help.

Best Regards,
Robin

0 件の賞賛
返信