S32K312 Port Update Code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 Port Update Code

1,057 Views
coo
Contributor I

I get this error when generating after setting up a port, where should I fix it so it doesn't happen?
I can fix it and use it, but I want to set it so that I don't get this error in the future.
I don't see any modifications in the component settings.

coo_0-1717030961163.png

 

0 Kudos
Reply
1 Reply

1,038 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Maybe it is caused by installing multiple versions of S32K3 RTD in S32DS v3.4.

If you installed both RTD RTM 1.0.0 and RTM 2.0.0, to avoid project RTD version auto conversion which would break up the old version projects, try to remove the  “compatibility.xml” 
located at “C:\NXP\S32DS.3.4\eclipse\mcu_data\configuration”"


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply