S32K312 PWM generation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K312 PWM generation

845 次查看
weiweichen
Contributor I

Hello,

I am facing the issue of PWM generation on the S32K.

The uC looks resetting when config frequency of PWM over 10kHz when the task is called in 10ms. 

  • It is possible to generate such frequency of PWM using a 10 ms task?
  • Do you have any workaround to resolve the issue?

(CORE_CLK = 120MHZ)

BR

Chen

0 项奖励
回复
1 回复

809 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @weiweichen 

Could you provide more information about the application and connfigurations?

 

BR, VaneB

0 项奖励
回复