S32K312 PWM generation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 PWM generation

802 Views
weiweichen
Contributor I

Hello,

I am facing the issue of PWM generation on the S32K.

The uC looks resetting when config frequency of PWM over 10kHz when the task is called in 10ms. 

  • It is possible to generate such frequency of PWM using a 10 ms task?
  • Do you have any workaround to resolve the issue?

(CORE_CLK = 120MHZ)

BR

Chen

0 Kudos
Reply
1 Reply

766 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @weiweichen 

Could you provide more information about the application and connfigurations?

 

BR, VaneB

0 Kudos
Reply