S32K312 PWM ICU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 PWM ICU

1,165件の閲覧回数
Zhuang
Contributor I

Hi NXP Teams,

When I capture pwm waveform in icu, using breakpoint running, I capture data is normal, if I directly run full speed and then pause, the captured data is abnormal.

And interrupt to a flag bit, and then step into the interrupt, the flag bit will be set to 1, direct full speed operation, the flag bit can not be set to 1

Can you give me some advice? Thanks

0 件の賞賛
返信
1 返信

1,148件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Zhuang,

I would need more information.

Do you use EMIOs and if so, which ICU mode?

Do you use RTD drivers or your own implementation?

Can you share the project or a simplified test project that would show the issue, and I could test it on my side?

 

Thank you,

BR, Daniel

 

0 件の賞賛
返信