LPSPI Manual Chip Select

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPSPI Manual Chip Select

3,584 次查看
Aravind_Vinas
Contributor II

Hi, I am trying to configure my SPI2 port for operation using processor expert. But I see that there are already designated CS pins for operation. Could I configure the TCR register with PCS[0:3] and initiate transfer and manually control another GPIO pin as CS by pulling low? If so, what is the effect on the pin specified in the PCS field of the TCR register?

标记 (3)
0 项奖励
回复
6 回复数

3,564 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is a possible but somewhat overcombined way. SPI transfer is initiated when CS is low but according CLK clock.

If you drive CS line manually by general purpose output, content of TCR[PCS] is irrelevant.

0 项奖励
回复

3,543 次查看
Aravind_Vinas
Contributor II

But the TCR[PCS] points to some CS line always. Which means the line being pointed will get low whenever a transfer is initiated. Or is there a configuration on the SPI registers where it can ignore the TCR[PCS] setting?

 
 
0 项奖励
回复

3,525 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, but it is internal signal. If there is no routing done by PORT module (this internal signal to pin), it does not have any relevance.

0 项奖励
回复

3,520 次查看
Aravind_Vinas
Contributor II

If I understand this correctly, if the pin is not routed as ALT function to serve as PCS using the PORT engine, then this TCR[PCS] shall not have any effect on the pin.

0 项奖励
回复

3,516 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you are right.

0 项奖励
回复

3,513 次查看
Aravind_Vinas
Contributor II

Kudos, thanks for the quick support!

0 项奖励
回复