S32K312 OpenSDA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,497件の閲覧回数
AnhNguyenDuc
NXP Employee
NXP Employee

Hello everyone, I have a question about S32K312.

Which UART, S32K312's OpenSDA used ? And what pins.

Thank you.

0 件の賞賛
返信
1 解決策
4,423件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please download through the link I sent you privately.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,416件の閲覧回数
Dr_Bubo
Contributor I

Hi Robin,

we have also started development with K312 therefore I would have interested on this link as well. Could you send it me too? 

0 件の賞賛
返信
4,394件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Bubo,

This file is not currently publicly available and you are advised to contact a sales representative. LoveEmbedded181 is colleague, so I sent him a link that can only be downloaded from the intranet.

Best Regards,
Robin

0 件の賞賛
返信
4,465件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi LoveEmbedded181,

Please download the S32K312EVB-Q172_HW_PackRevA1.zip and then you can find the information in S32K312EVB-Q172_PackRevA1_HardwareUserManual.pdf.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
4,443件の閲覧回数
AnhNguyenDuc
NXP Employee
NXP Employee

Hi Robin_Shen,

Can you give me a link to get .zip file

タグ(1)
0 件の賞賛
返信
4,424件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please download through the link I sent you privately.

0 件の賞賛
返信