S32K312 LPUART Rx FIFO buffer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 LPUART Rx FIFO buffer

1,580件の閲覧回数
mirkop345
Contributor I

If LPUART ISR is enabled with default FIFO and AUTOSAR then max 10kbps communication is possible otherwise Rx buffer overrun happens due to AUTOSAR overhead. I assume enabling FIFO buffer depth this issue will be solved and higher data tares would be possible.

I am wondering how I can  change in RTD or MCAL settings for Rx FIFO depth?

0 件の賞賛
返信
3 返答(返信)

1,513件の閲覧回数
mirkop345
Contributor I

I was wondering if this setting for FIFO buffer depth  is accessible  in MCAL or RTD libraries? As per AUTOSAR I can not access any MCU register directly but rather via access function?

0 件の賞賛
返信

1,494件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@mirkop345

The RX FIFO depth of Lpuart is fixed and cannot be set by the user.

0 件の賞賛
返信

1,535件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@mirkop345

You can find the following figure in the data sheet.

The size of the RX FIFO is limted.

Senlent_0-1733119304164.png

 

0 件の賞賛
返信