S32K312 Bus Error: IMPRECISERR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 Bus Error: IMPRECISERR

1,252件の閲覧回数
Glen_Wan
Contributor I

Hi,all

     i use S32K312 MCU, when code run calculate double data, trigger exception, not always occur.

 

when exception occured, 

BFSR register Value: 04: indicate it is a IMPRECISERR BUS error

ABSFR register Value: 0x0208: indicate it is AXIM bus error, error type is SLVERR

 

because IMPRECISERR BUS error  is async error, so when exception occur, the current PC not equal to trigger issue PC. S32K312 use Cortex-M7 which not provide interface to close write buffer to let IMPRECISERR BUS error change to PRECISERR BUS error.

 

could you pls Provide some analytical directions, thanks

 

0 件の賞賛
返信
0 返答(返信)