S32K311 SPI DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K311 SPI DMA

1,749 Views
Jon123
Contributor II

S32K311 is configured with SPI DMA, but if the DMA channels use 4 and 5, then SPI can trigger a DMA interrupt. If you use other channels, then it will not work. For example, channels 0, 1, 2 and 3 will not work. Use EB to configure it here, RTD3.0. I want to ask why. Thank you. If you want to project, I can upload it.

0 Kudos
Reply
2 Replies

1,703 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Jon123,

Can you please share the whole project, the configuration and the code?

 

Thank you,

BR, Daniel

0 Kudos
Reply

1,747 Views
Jon123
Contributor II
 
To add, what's interesting is that this will not happen to the S32K312
0 Kudos
Reply