S32K311 Lpuart_Lin Slave always returns RX_HEADER_ERROR / RX_OVERRUN_ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K311 Lpuart_Lin Slave always returns RX_HEADER_ERROR / RX_OVERRUN_ERROR

Jump to solution
3,730 Views
johns_chuang
Contributor III

Dear Team,

We are trying to enable the Lpuart_Lin (Slave) functionality on the S32K311, and we are referencing the example Lin_Ip_FrameTransfer_S32K344, using Lpuart_Lin_Ip_Init and Lpuart_Lin_Ip_GetStatus.

After the Master transmits a LIN frame:
[0x00, 0xFF, 0x80, 0x11, 0x6E]

The return status from Lpuart_Lin_Ip_GetStatus remains stuck at LPUART_LIN_IP_STATUS_RX_HEADER_ERROR.

Additionally, in the interrupt callback LpuartSlaveCallback, the status is always LPUART_LIN_IP_RX_OVERRUN_ERROR.

Do you have any suggestions on what we should check, or recommended changes we could try?

Thank you in advance for your support.

Best,

Johns

Tags (3)
0 Kudos
Reply
1 Solution
3,591 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @johns_chuang,

I finally managed to reproduce the issue during testing.

It turns out the problem was not related to the clock configuration after all.

I was able to replicate the issue on my EVB. To do so, I had to switch the LIN hardware to UART2 (PTD6, PTD7).

Once I removed all custom interrupt handling, the communication started working correctly.

 

danielmartynek_0-1752146622977.png

These are the changes: 

danielmartynek_1-1752146674941.png

You need to select the handler from Lpuart_Lin_Ip_Irq.c

danielmartynek_2-1752146718615.png

 

Regards,

Daniel

 

 

View solution in original post

10 Replies
3,592 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @johns_chuang,

I finally managed to reproduce the issue during testing.

It turns out the problem was not related to the clock configuration after all.

I was able to replicate the issue on my EVB. To do so, I had to switch the LIN hardware to UART2 (PTD6, PTD7).

Once I removed all custom interrupt handling, the communication started working correctly.

 

danielmartynek_0-1752146622977.png

These are the changes: 

danielmartynek_1-1752146674941.png

You need to select the handler from Lpuart_Lin_Ip_Irq.c

danielmartynek_2-1752146718615.png

 

Regards,

Daniel

 

 

3,493 Views
johns_chuang
Contributor III
Hi Daniel, Do you know why I can only read the first byte? The BUFFER_SIZE in LinLpuartPdu is set to 3, but I’m only able to read the first byte — the remaining two bytes are both 0.
0 Kudos
Reply
3,488 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @johns_chuang,

Please create a new thread and describe it in details.

0 Kudos
Reply
3,715 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @johns_chuang,

The RX_HEADER_ERROR you're encountering is likely due to a timing mismatch..

Have you had a chance to measure the LIN signal using an oscilloscope? 

 

I reviewed the system clock configuration in your test project and noticed that it is not set up correctly.

 

danielmartynek_1-1751445179432.png

 

If you want to have CORE_CLK = 48MHz, use Option D - Low-Speed Run mode (CORE_CLK @ 48 MHz), RM rev10, Table 162.

danielmartynek_0-1751445151989.png

 

Thank you,

BR, Daniel

0 Kudos
Reply
3,712 Views
johns_chuang
Contributor III

Hi Daniel,

Sorry, I’m still getting used to the S32DS interface.
Could you please explain in more detail what you meant by the system clock error?
How should I correctly configure it to 48 MHz?

Currently, I’m trying to receive 1 byte of LIN data:

LeCroy3.jpg

 

Eventually, I plan to work with 8 bytes of LIN data:

LeCroy4.jpg

 


Thank you for your support.

Best,

Johns

0 Kudos
Reply
3,702 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @johns_chuang,

Before we can proceed further, the system clock configuration must be corrected - use the S32DS GUI (configuration tool).

Please note that NXP does not guarantee the functionality of the MCU if the ratios between the system clock domains deviate from an approved configuration. Using unsupported clock settings may lead to unpredictable behavior.

danielmartynek_0-1751461552906.png

If your target is to run CORE_CLK at 48 MHz, you must configure all system clocks according to Table 162, Option D – Low-Speed Run mode (as per RM Rev. 10). 

 

Thank you,

BR, Daniel

 

0 Kudos
Reply
3,669 Views
johns_chuang
Contributor III

Hi Daniel,

Clock has been fixed, but the issue still persists. Could you kindly advise what I should check next? 

Thank you again for your support.

johns_chuang_0-1751508607543.png

 

MCU:S32K311

S32DS ver. 3.6.2

SDK:RlatformSDK_S32K3_S32K311_M7 v5.0.0

 

Best,

Johns

0 Kudos
Reply
3,619 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @johns_chuang,

I'm sorry for the delay.

What is the baud rate of the LIN signal? Can you measure that?

Also, can you share the LPUART_0 registers after initialization?

 

Thank you,

BR, Daniel

0 Kudos
Reply
3,616 Views
johns_chuang
Contributor III

Hi Daniel,

The LIN baud rate is 19200 bps.

Are you referring to the LPUART_0 registers shown in this image?

johns_chuang_0-1751969979358.png

 

Thank you for your help.

Best,

Johns

0 Kudos
Reply
3,723 Views
johns_chuang
Contributor III

Sorry, Sync was wrong. Correct LIN signal: [0x00, 0x55, 0x80, 0x11, 0x6E], ID is 0x00.

0 Kudos
Reply