S32K310 Locked

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K310 Locked

537 Views
Chenxu1
Contributor I

Hello, NXP experts! 
I am facing a troublesome problem:
When I used the S32DS project to download to the S32K310, it was able to run normally.
When I used the Mcal configuration project of the S32DS and downloaded it to the S32K310, the chip was locked. Look at the rst pin and see a reset signal every few milliseconds.We tried to disable the external 16M crystal oscillator and PLL, and using FIRC, we found that it would still be locked.
Q:Is there anything to note about Mcal configuration in the S32DS?

Chenxu1_0-1731057770608.png

 

 

0 Kudos
Reply
3 Replies

500 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

It seems that you are referring to the examples in the S32K3 LIN STACK. Which version of LIN STACK did you install? Which version of S32K3 RTD did you install?
I saw the Lin_Master_S32K311_Example_DS project in SW32K3_S32M27X_LIN_STACK_2.0.5_D2410.
Will there be any problems if you download this unmodified example on the S32K31XEVB-Q100 board?
In addition, your Mcu seems to have a warning. Please tell me what the warning is.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

497 Views
Chenxu1
Contributor I

Yes, I modified it with  the Lin_Master_S32K311_Example_DS project in SW32K3_S32M27X_LIN_STACK_2.0.5_D2410.
I only have S32K310 boards, so I can't test the original project.
Warning is as follows:

Chenxu1_0-1731303749421.png
If I set this option to enable, I get a clock error.

Chenxu1_1-1731303867576.png

 

 



0 Kudos
Reply

488 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I am able to run the Lin_Master_S32K311_Example_DS project of SW32K3_S32M27X_LIN_STACK_2.0.5_D2410 on S32K31XEVB-Q100 board.

Please check the configuration according to the differences between S32K310 and S32K311 mentioned in Table 1. S32K3xx chip's feature comparison of S32K3 Data Sheet.

different S32K311 S32K310.jpg

0 Kudos
Reply