S32K310 - C40_Ip Peripheral Cache Memory Support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K310 - C40_Ip Peripheral Cache Memory Support

2,465 次查看
SandyHCL
Contributor I

Hi NXP Team,

I am working on S32K310 controller and trying to configure the C40_Ip peripheral but it is throwing an error of Cache memory not supported. Refer to the attached screenshot. Is there any package I've missed to install? Kindly suggest.

Regards,

San

SandyHCL_0-1718885414941.pngSandyHCL_0-1718885414941.png

SandyHCL_1-1718885592895.pngSandyHCL_1-1718885592895.png

SandyHCL_2-1718885618079.pngSandyHCL_2-1718885618079.png

 

 

0 项奖励
回复
3 回复数

2,434 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @SandyHCL 

I deeply analyzed the platform support for the FLS driver features in User Mode, and the Synchronize Cache Feature is not supported by the RTD versions compliant with AUTOSAR 4.4. If you want to use this feature I would recommend using RTD versions compliant with AUTOSAR R21-11 as RTD version 3.0.0 P07. 

 

B.R.

VaneB

0 项奖励
回复

2,400 次查看
SandyHCL
Contributor I

Hi @VaneB ,

I've the Patch 07 installed already. Here are the screenshots of the packages installed in my laptop. Can you suggest what to do further?

SandyHCL_0-1719211360508.pngSandyHCL_0-1719211360508.pngSandyHCL_1-1719211402034.pngSandyHCL_1-1719211402034.png

Regards,

San

0 项奖励
回复

2,394 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @SandyHCL 

I am afraid that S32DS 3.5 has problems when has more than one RTD version installed, the suggestion is to uninstall all the RTD packages and reinstall only the ones with dependencies with the RTD 3.0.0 P07.

0 项奖励
回复