S32K3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
3,305 Views
hajianik
Senior Contributor I

Hi,

I have installed DS version 3.4 and S32K3XX DEVELOPMENT PACKAGE and S32K3 Real-Time Drivers AUTOSAR 4.4 Version 2.0.0 and  GCC 9.2 and GNUARM PEMICRO INTERFACE DEBUGGING SUPPORT.

I can build the examples by S32DS PROJEDTS FROM EXAMPLE tab.

However I couldn't flash the code nor debug the project.. for instance take a project called

"Dio_Example_S32k3xx" I use a debug configuration called "Dio_Example_S32k3xx "Dio_Example_S32k3xx_debug_flash_ PNE".

WITH THIS DEBUG CONFIGURATION , open sda does not even connect to the target  and When I use JTAG and PNE debugger it connects to the target and then display a "run time error" message and debugging terminates. I'm using  a S32K1XEVAL-Q100 Board.

Please help me to resolve this.

Thanks,

Koorosh Hajiani

Tags (1)
0 Kudos
Reply
1 Solution
3,217 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @hajianik,

There is support for S32K311 in S32DS IDE v3.5, RTD 3.0.0

There are no RTD examples for S32K311, but a new RTD project for S32K311 can be created.

danielmartynek_0-1691397951334.pngdanielmartynek_0-1691397951334.png

 

Regards,

Daniel

 

View solution in original post

0 Kudos
Reply
3 Replies
3,249 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @hajianik,

According to your description, you use S32K3 RTD and S32K1 board.

If this is a typo, and it is an S32K3 board, then, there is no OpenSDA debugger.

Can you clarify?

 

Thank you,

Daniel

 

 

0 Kudos
Reply
3,239 Views
hajianik
Senior Contributor I

Hi Daniel,

It is a typo and I use S32K3-q100 board. on this board the processor is s32k311q100 however the examples are   targeted for a s32k312_q172 micro .when I use these examples that are  for s32k312_q172 I get a  an exception in start_up code, that is when I use external power supply and PNE debugger.

There is no support in DESIGN STUDIO V3.4 for s32k311 or 310 series   . WHAT CAN I DO?

 

Thanks.

0 Kudos
Reply
3,218 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @hajianik,

There is support for S32K311 in S32DS IDE v3.5, RTD 3.0.0

There are no RTD examples for S32K311, but a new RTD project for S32K311 can be created.

danielmartynek_0-1691397951334.pngdanielmartynek_0-1691397951334.png

 

Regards,

Daniel

 

0 Kudos
Reply