S32K3 frequency measurement on FLEXio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K3 frequency measurement on FLEXio

跳至解决方案
474 次查看
Tobias12
Contributor I

Hi all,

I am looking for a possibility to measure frequencies on the S32K FLEXios. Unfortunately EMIOS has not enough channels for my application.

The goal is to measure frequencies up to 20kHz.

Is it possible to use the FLEXios or is there another option I don't see?

 

Thanks

Tobias 

0 项奖励
回复
1 解答
450 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Tobias,

There are just EMIOs and the FlexIO for HW input capture.

The FlexIO input capture is used in emulated SENT receiver (RM, 73.6.8 SENT receiver).

There are SENT receiver examples in RTD, so you can refer to that.

 

Regards,

Daniel

 

在原帖中查看解决方案

1 回复
451 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Tobias,

There are just EMIOs and the FlexIO for HW input capture.

The FlexIO input capture is used in emulated SENT receiver (RM, 73.6.8 SENT receiver).

There are SENT receiver examples in RTD, so you can refer to that.

 

Regards,

Daniel