S32K3 frequency measurement on FLEXio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 frequency measurement on FLEXio

Jump to solution
304 Views
Tobias12
Contributor I

Hi all,

I am looking for a possibility to measure frequencies on the S32K FLEXios. Unfortunately EMIOS has not enough channels for my application.

The goal is to measure frequencies up to 20kHz.

Is it possible to use the FLEXios or is there another option I don't see?

 

Thanks

Tobias 

0 Kudos
1 Solution
280 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Tobias,

There are just EMIOs and the FlexIO for HW input capture.

The FlexIO input capture is used in emulated SENT receiver (RM, 73.6.8 SENT receiver).

There are SENT receiver examples in RTD, so you can refer to that.

 

Regards,

Daniel

 

View solution in original post

1 Reply
281 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Tobias,

There are just EMIOs and the FlexIO for HW input capture.

The FlexIO input capture is used in emulated SENT receiver (RM, 73.6.8 SENT receiver).

There are SENT receiver examples in RTD, so you can refer to that.

 

Regards,

Daniel