S32K3 driver for Micro-second-channel MSC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 driver for Micro-second-channel MSC

Jump to solution
1,358 Views
francescovico
Contributor III

Hello,

I need to implement HW and SW to drive an IC that Micro-second-channel MSC.

Which are best solution HW and SW to implement this communication using S32K3 microcontroller?

Regards, Francesco. 

0 Kudos
Reply
1 Solution
1,309 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @francescovico 

Currently, there is no support or implementation for MSC on the S32K3xx family. However, based on the understanding of the protocol, one possible approach for MSC implementation on S32K3xx might involve using the LPSPI module to emulate MSC behavior. Since MSC is based on SPI but includes additional timing and synchronization features.

Please note that this is not an officially supported solution. It is a suggestion based on protocol characteristics, and we do not provide support for MSC on the S32K3xx. The functionality of such an implementation would depend entirely on your own development.

Additionally, there is a discussion at the following link , you will find a discussion describing an MSC implementation example for the MPC5744P. While this example is not directly compatible with the S32K3xx, it may serve as a helpful reference if you want to consider an alternative devices that better align with your requirements.

some questions about Timed serial Bus(TSB) and Microsecond Channel downstream(MSC)

 

BR, VaneB

View solution in original post

0 Kudos
Reply
1 Reply
1,310 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @francescovico 

Currently, there is no support or implementation for MSC on the S32K3xx family. However, based on the understanding of the protocol, one possible approach for MSC implementation on S32K3xx might involve using the LPSPI module to emulate MSC behavior. Since MSC is based on SPI but includes additional timing and synchronization features.

Please note that this is not an officially supported solution. It is a suggestion based on protocol characteristics, and we do not provide support for MSC on the S32K3xx. The functionality of such an implementation would depend entirely on your own development.

Additionally, there is a discussion at the following link , you will find a discussion describing an MSC implementation example for the MPC5744P. While this example is not directly compatible with the S32K3xx, it may serve as a helpful reference if you want to consider an alternative devices that better align with your requirements.

some questions about Timed serial Bus(TSB) and Microsecond Channel downstream(MSC)

 

BR, VaneB

0 Kudos
Reply