S32K3 core power down error & running(bus error)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 core power down error & running(bus error)

8,686 Views
kjy106906
Contributor IV

I ask what state the MCU is in and what cases occur in the following situations.

What's interesting is that if I run a specific function with Over(Trace32), the issue occurs, but when I run it with Step(Trace32), the issue does not occur.

(Power is being supplied to the MCU normally.)

kjy106906_0-1713939415180.png

 

Tags (1)
0 Kudos
Reply
15 Replies

4,057 Views
Palacni
Contributor I

Hello all

We are currently facing the same kind of issue on our project. CRC and C40 modules are not used, however everything else that is described in this topic is valid in our case.

@kjy106906 , have you solved your issue ?

Edit: @danielmartynek , since this topic, have you ever heard of this kind of issue that has been resolved ?

Thank for your answers

0 Kudos
Reply

1,210 Views
seasonedbit
Contributor II

@kjy106906 ,

@danielmartynek ,

The same question were you able to find the root cause?

 

This issue is also observed with size optimizations and goes away if no optimization is used.

0 Kudos
Reply

1,197 Views
Palacni
Contributor I

Hello,

We were finally able to identify the root cause of the issue on our side.

It was linked to NXP errata ERR052460, related to branch speculation. The following code snippet corrects the behavior.

    // NXP ERR052460 Workaround: Cortex-M7: A hang scenario can occur when a reserved read locked memory region is accessed by application cores
    *((uint32_t*) 0x402AC0F0) = 0x1CB0499Du;
    *((uint32_t*) 0x402AC0F0) = 0xB9920D38u;

I’m not sure whether this is the exact same root cause on your side (I’m not from NXP and it seems they won’t respond anyway), but it’s worth checking.

 

1,068 Views
seasonedbit
Contributor II

@Palacni Thank you very much for your prompt reply. Unfortunately on my derivate there is another peripheral at the location cited by errata to enable user access. I've asked NXP for errata of my relatively new derivate .......... . . .

It works when any one of the following is used,

  1. Disable the optimizations (-O0)
  2. Use SRAM of another domain on the SoC
  3. Disable the Instruction cache
  4. Stepping in via debugger
0 Kudos
Reply

8,675 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @kjy106906,

Can you be more specific?

What function do you step over here?

Can you also specify the MCU and RTD version if you use it?

 

Thank you,

BR, Daniel

0 Kudos
Reply

8,668 Views
kjy106906
Contributor IV

Thank you always @danielmartynek 

That function is not an RTD function but a simple calculation function.
An issue occurs when calculating the CRC of C40 read data at a specific address.
This occurs when executing the CRC calculation function, not when reading.
MCU: S32K312, RTD version: 2.0.0

 

I wonder what state the MCU is in and the reason for entering that state.

 

0 Kudos
Reply

8,662 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @kjy106906,

Please find more information about the fault exception.

Refer to these documents:

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447

https://community.nxp.com/t5/S32K-Knowledge-Base/How-To-Debug-A-Fault-Exception-On-ARM-Cortex-M-V7M-...

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Handling-Interrupt-DS3-5-...

Read Configurable Fault Status Register (CSFR) and Bus Fault Address Register (BFAR) if BFARVALID = 1. You should be able to find the PC address of the fault instruction on the stack.

 

Regards,

Daniel

 

 

 

 

0 Kudos
Reply

8,632 Views
kjy106906
Contributor IV

Thank you

Even if I set a break on the error handler, the break does not occur and the MCU enters the corresponding state.

 

I wonder what state the MCU is in and the reason for entering that state.

0 Kudos
Reply

8,623 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @kjy106906,

So, I understand the core does not detect any fault exception, it does not go to the HardFault_Handler().

Can you monitor the reset_b pin? Is the application running?

If so, it might be a lauterbach issue.

 

BR, Daniel

 

0 Kudos
Reply

8,519 Views
kjy106906
Contributor IV

Thank you @danielmartynek 

I am currently using Vector Microsar
The MCU does not enter any Os Hal Fault (Exception).
If an MCU Exception is entered, I think I will see the MCU jumping to the corresponding code in the debugger, but currently a Bus error is output in Trace32.
Therefore, it seems that an exception did not occur.
If there are any more points to check, let me know.


Neither Reset_b nor VDD_HA_A fall to Low.

This issue causes infinite SBC reset in BMS-only state without Trace32. Because that issue occurs in Dataflash Init, the MCU does not operate and an infinite reset of the SBC occurs.
So it's not a lauterbach issue either.

It's an important issue for us. Please let me know if there are any more points to check.

0 Kudos
Reply

8,508 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @kjy106906,

I would like to test it on my side.

Can you share the project?

Or preferably a simplified version with .elf that can reproduce the issue?

If you don't want to share it here, create a ticket.

 

Thank you,

Daniel

 

0 Kudos
Reply

8,498 Views
kjy106906
Contributor IV

Thank you @danielmartynek 

Sharing the entire project is not possible due to company security reasons.
Even if I share my elf, it currently works on my board.
Testing may not be possible in your environment.

It is also not possible to share the simplified elf.
Strangely, even if I add a few lines of unnecessary code (adding a while statement for debugging, adding a global variable, etc.), the issue does not reproduce.

Currently, this issue has occurred in 5 BMS boards.
It's all related to Dataflash.
Could the above phenomenon occur due to dataflash area being broken or other errors?

0 Kudos
Reply

8,471 Views
danielmartynek
NXP TechSupport
NXP TechSupport

When you read the DFlash, do you use the driver?

Because the driver checks for errors:

danielmartynek_0-1714660282009.png

 

Thank you,

Daniel

0 Kudos
Reply

8,463 Views
kjy106906
Contributor IV

Thank you @danielmartynek 

 

I'm also using the C40 library. (C40_Ip_Read)
However, Error is not returned, ( Success is returned.)

0 Kudos
Reply

8,412 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @kjy106906,

You wrote: "Strangely, even if I add a few lines of unnecessary code (adding a while statement for debugging, adding a global variable, etc.), the issue does not reproduce."

If you write registers or an sram memory, can you read it back so that all the operations are properly serialized?

RM, rev.8, Section 3.8 Serialization of memory operations.

 

Regards,

Daniel

0 Kudos
Reply