S32K3: Wake issues from Standby mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3: Wake issues from Standby mode

1,502件の閲覧回数
himonkoch
Contributor III

Hi,

I am trying to wake up my MCU (S32K312 EVB) from Standby Mode using an external GPIO wake source.
When the wake up signal is a rising edge the wake up is successful.
When the wake up signal is a falling edge then the wake is NOT WORKING as expected.


The symptoms that I observe:  micro-controller wakes up immediately after getting into standby mode. This happens only when the wake source [Wkpu: IcuDefaultStartEdge] is configured as FALLING_EDGE or BOTH_EDGES. In the case wake source is configured as  RISING_EDGE wake works fine as expected (gets into standby mode and wakes up only when triggered).

I am not able to figure out why the wake method is not working in the case of Falling_edge config.

Any inputs will be of great help on this.

Thanks in advance.

S32K312EVB-Q172

 

 

タグ(4)
0 件の賞賛
返信
1 返信

1,473件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @himonkoch,

I can see you also have an open support ticket. In order to avoid any miscommunication, I will be supporting your issue through the internal case.

Best regards,
Julián

0 件の賞賛
返信