S32K3 SWT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,989件の閲覧回数
Jackson_Ping
Contributor II

Hi,all,

   I've recently been learning the routines for software watchdog, but I can't find the API function for feeding the dog. On the GUI, I set the "Operation Mode" in the quick mode to the immediate restart mode and set the timeout period to 2s.

  I would like to ask if the API for feeding dogs is' Wdg_43_Instance0_SetTriggerCondition '? If not, can you give some good advice? Thank you very much!

 

微信图片_20240102114552.png

 

微信图片_20240102114715.png

Best Regards,

Jackson Ping

 

0 件の賞賛
返信
1 解決策
2,972件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I do not know to which driver you are referring, but it should be always in driver documentation.

Looking at RTD v4.4 1.0.0 I can read:

petervlna_1-1704185382902.png

Best regards,

Peter

 

元の投稿で解決策を見る

2 返答(返信)
2,973件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I do not know to which driver you are referring, but it should be always in driver documentation.

Looking at RTD v4.4 1.0.0 I can read:

petervlna_1-1704185382902.png

Best regards,

Peter

 

2,933件の閲覧回数
Jackson_Ping
Contributor II

Hi,Peter,

 

Thanks for your answer, I have solved the problem.

 

 

Best regards,

Jackson

 

0 件の賞賛
返信