S32K3 RTD driver project setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 RTD driver project setting

1,593 Views
StephenYeh
Contributor III

Hi,

Is it possible that the Design Studio 3.4 (Install RTD 2.0.0 and RTD1.0.0) to build sample code whatever the RTD 1.0.0 or RTD 2.0.0?

I can load the RTD2.0.0 sample code and build without fail, but RTD1.0.0(NXP provide the reference sample code is based on RTD100 version) sample code will build error.

 

 

 

 

Tags (1)
0 Kudos
Reply
1 Reply

1,573 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@StephenYeh

This is a known issue, you can refer to this article.

This article is in Chinese, please let me know if you have any language issues.

Notice for Upgrade K3 RTD from 1.0 to 2.0

https://community.nxp.com/t5/S32K-Knowledge-Base/Notice-for-Upgrade-K3-RTD-from-1-0-to-2-0/ta-p/1489... 

BR!

     Jim,

0 Kudos
Reply