Mass erase not disable security

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mass erase not disable security

915 Views
lyz
Contributor II

i configure FSEC register by follow figure:

lyz_0-1670207157572.png

lyz_5-1670208069902.png

 

example code as follow:

lyz_2-1670207557076.png

inside, 

lyz_3-1670207649072.png

mass erase enable, now, chip is secure. but now,

lyz_4-1670207761601.png

mass erase not disable security. option as follow:

lyz_6-1670208305649.png

button yes, not disable security.

unlock kinetis commander also disable security. 

please tell me why? Thanks

0 Kudos
Reply
1 Reply

909 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi lyz,

Have you tried the new version of J-Flash software? Did you select allow security when chose device?
Mass erase should be able to unsecure the chip.
Please read the value of MDM-AP status and control registers by refer to:https://community.nxp.com/t5/S32K/Unbricking-S32K146/m-p/937227
Please input connect command first.
You can also try program the chip after mass erase using the loadbin command.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply