S32K3 RTD driver project setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 RTD driver project setting

1,562件の閲覧回数
StephenYeh
Contributor III

Hi,

Is it possible that the Design Studio 3.4 (Install RTD 2.0.0 and RTD1.0.0) to build sample code whatever the RTD 1.0.0 or RTD 2.0.0?

I can load the RTD2.0.0 sample code and build without fail, but RTD1.0.0(NXP provide the reference sample code is based on RTD100 version) sample code will build error.

 

 

 

 

タグ(1)
0 件の賞賛
返信
1 返信

1,542件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@StephenYeh

This is a known issue, you can refer to this article.

This article is in Chinese, please let me know if you have any language issues.

Notice for Upgrade K3 RTD from 1.0 to 2.0

https://community.nxp.com/t5/S32K-Knowledge-Base/Notice-for-Upgrade-K3-RTD-from-1-0-to-2-0/ta-p/1489... 

BR!

     Jim,

0 件の賞賛
返信