S32K3 PWM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 PWM

2,353件の閲覧回数
Jackson_Ping
Contributor II

Hi,all,

I am currently using the S32K324 chip.I have two urgent questions:

1.Whether the two PWM channels can be associated, the period is the same, but the phase difference is set

2.Can the PWM phase of eMIOS be synchronously controlled by an external trigger source?

Thanks!

Best Regerds,

  Jackson

0 件の賞賛
返信
2 返答(返信)

2,335件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) There is no easy way to do this, if there is ever any, depends on used shift, duty cycle, its update need and mode used. If the shifting is done within a PWM period there is no issue with OPWMB mode for sure. For the case when crossing boundary it cannot work for sure. One way could be changing the polarity and recalculate match values. Most probably this will bring some SW overhead and possible glitches on polarity changes, I guess. Another way could be using an DAOC mode and update A and B registers (thus re-enable comparators) with the help of DMA, for example.
If the phase shift is not changing you can use OPWFMB mode and init the CTN register by shifted value when PWM generators are disabled, as mentioned in https://community.nxp.com/thread/449233.
But for phase shift change the PWM must be stopped then.

2) there is no synchronization between module counters in terms the counter will be reinit at other channel match/capture or similar. Counters can be just started at the same time using global prescaler

BR, Petr

0 件の賞賛
返信

2,234件の閲覧回数
Jackson_Ping
Contributor II

Hi,PetrS,

 

Thanks for your suggestion.

 

Best Regards,

 Jackson

0 件の賞賛
返信