S32K3 LPCMP module propagation delay issues of Trigger mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K3 LPCMP module propagation delay issues of Trigger mode?

1,205 次查看
zhanguiyang
Contributor I

zhanguiyang_0-1683433152098.png

When NSAM=0, is this the location where sampling occurs?

If that's the case, I think it's unreasonable because the sampling value at this point is not the result of the selected channel 1.

0 项奖励
回复
2 回复数

1,157 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @zhanguiyang,

It is under an internal discussion,

I will update the thread as soon as possible,

 

Regards,
Daniel

0 项奖励
回复

1,081 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @zhanguiyang,

It has been confirmed by the design team that NSAM can be set to 0 in this mode.

The sampling can start at the time the channel is selected.

 

Regards,

Daniel

0 项奖励
回复